Archive

How much energy are your drives saving?

2009-08-27 - ABB drives are now equipped with a built-in energy efficiency calculator that continuously measures how much energy the drive is saving, the value of the saving in local currency and the reduction in carbon dioxide emissions that the drive has achieved.

Innovative software helps welding robots save materials and energy

2009-08-18 - Teaching robots to weld with the skill of a human worker is easier said than done, but ABB's VirtualArc software allows operators to perfect the welding procedure from their desks, without tying up the robot or wasting resources through real-life trial and error

ABB control system helps turn food waste into fuel

2009-08-18 - Small bioethanol plants in Finland are using local food waste to make a low-carbon gasoline and help reduce greenhouse gas emissions from cars and trucks. ABB’s Extended Automation System 800xA is making it possible.

ABB technologies that changed the world
Part four: substations

2009-08-07 - As the world's leading supplier of electrical substations, ABB has delivered key advances that have improved the reliability and flexibility of transmission and distribution systems in the most demanding environments, from deserts and mountains to offshore rigs and city centers.

ABB solution will monitor and manage dozens of hydro plants in North America

2009-08-04 - ABB is supplying a network management solution that will monitor and control 134 renewable energy facilities that provide states and provinces across Canada and the United States with clean, emission-free power.

ABB solution greens global shipping

2009-07-24 - A pioneering ABB solution that cuts greenhouse gas emissions and reduces ship fuel costs has helped the major North Sea port of Gothenburg win its second international award for cleaning up shipping and the seas.

European companies support vision to tap desert solar

2009-07-13 - A group of European companies will meet this week to inaugurate the Desertec Industrial Initiative and discuss an idea proposed by ABB in the early 1990s: harnessing solar power from deserts to deliver emission-free electricity to Europe.

Singapore’s used-water superhighway

2009-07-03 - One of the world’s largest and most innovative water treatment projects is the Changi water reclamation plant, opened in June by the Public Utilities Board, Singapore's national water agency. The plant at the heart of Singapore's massive deep tunnel sewerage system is powered in large part by ABB.

ABB in 3D at Nor-Shipping

2009-06-29 - ABB’s three dimensional animations created a stir at the Nor-Shipping Exhibition in Lillestrøm, Norway in mid-June, while ABB's next generation Azipod was a featured product.

ABB technology will help bring drinking water to millions in Algeria

2009-06-23 - An ABB solution for the world’s largest seawater desalination plant using reverse osmosis technology – currently under construction in Algeria - will boost energy efficiency and cut maintenance downtime from weeks to days compared to current industry benchmarks.

Archive selection